9/18/2017 2:50 PM | |
Joined: 5/7/2015 Last visit: 2/14/2023 Posts: 55 Rating:
|
Hi Experts, I have a similar problem. In my present project I have a ET 200S on IM-151-3AA23-0AB0 (v7.0.5) driven by a CPU 1215 C DC/DC/DC v4.2.0. I am attempting without success to configure the PLC using TIA v13 SP2. The hardware catalog simply does not have V4.2 PLC. The error messages that show up in the diagnostic buffer are.. "Hardware component removed or Missing" "Hardware component removed or missing - internal application reasons" " Hardware component not available due to type mismatch" All these I presume are due to Step7 v13 SP2 + CPU v 4.2 Will welcome any help to solve this issue. Thanks and regards ------------------------------------------------------------------------------------------ AttachmentDiagnostics.txt (30 Downloads) |
Last edited by: Jen_Moderator at: 9/19/2017 10:02:09 AMNew subject after splitting |
|
Follow us on