2/15/2020 2:20 PM | |
Joined: 6/14/2015 Last visit: 4/25/2024 Posts: 236 Rating: (1) |
HI every body. I want to connect ET200M to s71200 cpus. Is it possible? |
2/15/2020 3:12 PM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (818) |
Hello, no. It's S7-300/400 interface system. |
With best regards... |
|
2/15/2020 3:16 PM | |
Joined: 6/14/2015 Last visit: 4/25/2024 Posts: 236 Rating: (1) |
I want to connect them with profinet not direct |
2/15/2020 3:25 PM | |
Joined: 9/27/2006 Last visit: 4/25/2024 Posts: 12257 Rating: (2665) |
Hello akbar; Yes you can, very easily. Do you want to use Profinet or Profibus connections? You can setup an ET 200M station as a Profinet IO Device using an IM 153-4 head station (connected to the Profinet integrated port of the CPU); for Profibus you will need a IM 153-2 (Profibus head station on the ET 200M, and a CM 1243-5 as DP master in the S7-1200 rack. Both IMs are available in the network catalog of Step 7 v1x. Look at the pdf prepared by our friend jklm in the following discussion, it gives screenshots of both possibilities: ET 200M as Profinet IO Device, ET 200M as Profibus slave., with a S7-1200 CPU. https://support.industry.siemens.com/cs/ww/en/view/109752566 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 02/15/2020 15:28:12 |
|
2/16/2020 6:00 AM | |
Joined: 6/14/2015 Last visit: 4/25/2024 Posts: 236 Rating: (1) |
Thanks so much. I have analog and digital I/O. also I have FM modulus (SIWAREX : 7MH4 950-2AA01 ), can I use FM modulus and analog modulus? |
2/16/2020 11:52 AM | |
Joined: 9/27/2006 Last visit: 4/25/2024 Posts: 12257 Rating: (2665) |
Hello akbar; When you select the specific IM 15x-y you Will use for your ET 200M in the hardware configuration, open the subdirectory of that IM to select all analog and digital I/O modules you need to build your ET 200M station. The configuration must match the existing station it will connect to. The Siwarex U module you want to use will work inside a ET 200M station, see this description from Product Support, below.And the following download shows how to use your Siwarex U in different versions of TIA Portal: https://support.industry.siemens.com/cs/ww/en/view/28391777 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 02/16/2020 16:06:41 |
|
2/18/2020 6:15 AM | |
Joined: 6/12/2016 Last visit: 6/4/2022 Posts: 5 Rating: (0) |
You can connect s7-1500 to FM with IM153-4 in PORTAL V13 SP2 |
I LOVE SIMATIC GAME |
|
12/30/2020 7:20 PM | |
Joined: 6/14/2015 Last visit: 4/25/2024 Posts: 236 Rating: (1) |
thanks so much. you mean I can use any module 300 in ET 200M station that connected with s7-1200. Am I right? |
12/30/2020 9:32 PM | |
Joined: 9/27/2006 Last visit: 4/25/2024 Posts: 12257 Rating: (2665) |
Hello Akbar; Unfortunately, a bit more research on the forum has brought me to this document that states the Siwarex U module cannot be integrated to a S7-1200: Is it possible to integrate a SIWAREX U, CS, FTA or FTC into a S7-1200 system? https://support.industry.siemens.com/cs/us/en/view/54688602 In the following discussion, our specialist Siwarexi proposes alternatives to the Siwarex U, when your CPU is a S7-1200: the Siwarex 231, mounted next to the S7-1200 CPU. https://support.industry.siemens.com/cs/ww/en/view/109780855/62537505931 Hope this helps, |
Follow us on