2/7/2016 10:09 AM | |
Joined: 2/5/2016 Last visit: 6/28/2022 Posts: 20 Rating:
|
i have PCS7 system consist of two redundant servers and three clients . the two redundant serves connect to four AS (S7 400 redundant each PLC has its CP).each one of the two servers connect to the four AS by industrial Ethernet card CP1613 using ISO protocol and connection type S7 connection fault-tolerant .the link type between the two servers and the Four AS is fiber and it is needed to add another wireless link using 3G gateways for each AS as redundant link. To access the AS through the 3G gateway , we have to use the IP address of the 3G gateway . So now to access the AS through the wireless link , i have to use the gateway IP address and to use the fiber link , i have to use the iso protocol . How this two redundant link can be configured? AttachmentSiemens ISSUe.zip (32 Downloads) |
2/8/2016 11:42 AM | |
Joined: 3/14/2008 Last visit: 8/10/2024 Posts: 2082 Rating:
|
A wild guess... Is everything connected to the same network? Have you set your PG/PC interface to "PC Internal"? |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on