1/9/2019 3:45 PM | |
Joined: 5/27/2015 Last visit: 3/25/2024 Posts: 60 Rating: (26) |
Hi Ali, You have to: - Install SIMATIC NET on your system (is either on the same DVD as WinCC or on a separate one within the installation package of WinCC) - Check the PG/PC interface There is also an FAQ with a video which explains the steps: Why is the connection from WinCC to the S7 controller not established via TCP/IP? Best regards |
Follow us on