11/8/2012 4:36 AM | |
Posts: 3 Rating: (0) |
I'm a new member ! please show me the way to connect WinCC v7.0 sp2 with Excel 2007 ! thankyou all ! |
11/8/2012 2:07 PM | |
Posts: 1530 Rating: (59)
|
Hello lucphong126, could you tell me please what you want to do exactly. Do you want to export data in Excel? You may also try to use field "Search" here on this side an type in your catchwords. You will get lot of good information, e. g. FAQs. One example I will add here, maybe it'scomes already near tothat, you want to do: How can WinCC exchange data with Microsoft Excel or Access? Best regards Bizur |
This contribution was helpful to1 thankful Users |
11/13/2012 12:36 PM | |
Posts: 1530 Rating: (59)
|
Hello lucphong126, sorry, that my first answer didn't help you. I suppose the problem you had is, that my links works quite fine, but it is not the answer you needed, is this right or han't it been working at all? So I have to give you some other information: What options are there in WinCC for read and write access to TagLogging/AlarmLogging archives? This FAQ also contains information about WinCC Report Designer. Best regards Bizur |
11/16/2012 3:43 AM | |
Posts: 3 Rating: (0) |
Dear Bizur ! I only want to conect data beetwen WinCC and Excel or Access ! Anyway, thank for your enthusiasm !!! |
7/13/2015 7:07 AM | |
Joined: 10/3/2010 Last visit: 5/8/2024 Posts: 1552 Rating: (188) |
The example script above says on top: Sub OnLButtonDown(Byval Item, Byval Flags, Byval x, Byval y) so it means this script is executed on Press Left Mouse Click of a button on your pdl for example. |
B r g d s , |
|
This contribution was helpful to1 thankful Users |
Follow us on