6/15/2016 11:54 AM | |
Posts: 1 Rating: (0) |
Hi Oreca, I am beginner in PCS 7. Canyou please tell me which one of Countoh out I have to connect with Selfp1 .. Ms_Release other otherthing
------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 6/15/2016 12:06:34 PMNew subject after splitting |
|
6/15/2016 12:44 PM | |
Joined: 3/14/2008 Last visit: 5/14/2024 Posts: 2066 Rating: (928)
|
Hi there, It does not matter which output of countoh you connect to SelFp1, because this is an ANY parameter. When you compile the OS, the SelFp1 receives a jump attribute, which will lead to your connected block. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on