11/17/2012 10:10 AM | |
Joined: 12/27/2006 Last visit: 4/27/2024 Posts: 1196 Rating: (113) |
For an example look in the attachment. You must self make it better. So its not good for your motor to go quick from Forw, Quick stop, and then go REW. You must make timers in the programm, so your motor kan run-out, before you start again. Thats easy to make I think.... the outputs must be different. Normaly its 2 outputs for chanche direction, and 2 outputs for speed. p.e Output 1 = Forw and Output2 = Rew Output 3 = Slow, output 4 = Fast Also posibility is NOT Output 3 = Slow, OUTPUT 3 = Fast Good luck Attachmentmotorspeed.zip (194 Downloads) |
11/17/2012 7:58 PM | |
Posts: 4 Rating: (0) |
Hi, I've attached the program i made to work.I think it is far too complicated BUT it does do everything i want. AttachmentArtofex Kneader Example.zip (182 Downloads) |
11/17/2012 11:01 PM | |
Joined: 9/6/2008 Last visit: 3/29/2024 Posts: 134 Rating: (16) |
take a look in the sample , maybe it helps you. AttachmentBRED MIX.zip (184 Downloads) |
http://electrotech-techblogg.blogspot.gr/ |
|
11/20/2012 6:07 PM | |
Joined: 9/6/2008 Last visit: 3/29/2024 Posts: 134 Rating: (16) |
flags are in need when your programa actualy loop betwen operations . AttachmentBRED MIX.zip (194 Downloads) |
http://electrotech-techblogg.blogspot.gr/ |
|
This contribution was helpful to1 thankful Users |
Follow us on