5/18/2010 12:56 PM | |
Posts: 21 Rating: (0) |
Dear Sir/Madam, |
5/18/2010 3:55 PM | |||||
Joined: 9/27/2006 Last visit: 9/19/2024 Posts: 12282 Rating: (2684) |
Hello Patrick; The CP 441 (either -1 or -2) is designed for PtP communications, with add-on interfaces for RS-232, RS-422/485 or TTY. here is part of the description of the modules as shown in the A&D Mall: https://mall.automation.siemens.com/GB/guest/index.asp?aktPrim=0&nodeID=5000093&mlfb=6ES7441%2D1AA04%2D0AE0&aktTab=4&lang=en (look at the Description tab) · For powerful, high-speed serial communication via point-to-point connections · 2 versions: However, the S5-95U is a very small CPU, and I am wondering if a S7-400 is an overkill in this situation, if you are planning a one-to-one conversion. You could look at the compact CPUs of the S7-300 family, some of these CPUs come with a PtP port and dedicated communication functions, along with integrated I/Os and technological functions: the S7-313C-2 PtP and the S7-314C-2 PtP, with a RS-422/485 port and ASCII, 3964R and RK512 protocols inbuilt, which should be very close to the configuration of your S5-95U.
Hope this helps, Daniel Chartier |
||||
Last edited by: dchartier at: 5/18/2010 4:05 PM |
|||||
This contribution was helpful to1 thankful Users |
5/19/2010 10:18 AM | |
Joined: 10/7/2005 Last visit: 9/20/2024 Posts: 3021 Rating: (1054)
|
Hello Patrick_Sthlm what makes you think that it is a SINEC L1 link (I can not find any "SL1" entry in your DB1)? As far a I can see,SI2 is configured for 3964(R) protocol in DB1(see "RKT" entry in DB1 and chapter 3 of THIS manual), which is supported by S7 serial cards (SINEC L1 is however not as you already know). Question: What's connected to the other end of the serial link? I hope this helps |
Cheers |
|
Follow us on