1/26/2017 7:04 PM | |
Posts: 1 Rating: (0) |
Dear all pls help me out to convert this s5 program to s7 300 with cpu 318-2dp after few month started reading all the topics from this forum and tried to convert but ended with errors and warning since iam not familiar with s5 STL programming I request anyone to help pls find my s5 program backup taken from one of my plant Attachmentginnerplant.zip (181 Downloads) |
1/27/2017 10:02 AM | |
Joined: 7/9/2015 Last visit: 8/30/2024 Posts: 3943 Rating: (585) |
Hi, sorry, I have also less expirience in converting S5 to S7 but I hope these links could help you: From S5 to S7 Converter ManualSIMATIC STEP 7 V5.5 From S5 to S7Hope this helps you a little bit! Regards |
|
|
This contribution was helpful to2 thankful Users |
1/27/2017 10:58 AM | |
Joined: 2/22/2008 Last visit: 9/13/2024 Posts: 57 Rating: (6) |
Dear raj_1974, I suggest you to follow strictly all the recommendation mentioned in this manual, as our colleague posted above. From S5 to S7 Converter ManualImportant points 1. Prepare a table list with all new relevant DB's, FB's and FC's. This is the most important thing that you need to have in mind to avoid mistakes later on. 2. Convert you software and check detailed every code. You will have to find out all important codes that use indirect addressing. This will not be converted and you will spend a lot of time rewriting it. 3. Test every single function to make sure the are working as before. It is also important to check all fixed values when manipulating pointers in the software. 4. If you have problems when rewriting one piece of code, please post it here in the forum that everybody will try to help as far as possible. Hope it helps. Good luck! |
Best Regards |
|
This contribution was helpful to1 thankful Users |
1/27/2017 5:27 PM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (308)
|
Hello raj_1974 As well advised by Towome andRonaldo Junior , please go through the Manuals advised by them and follow them. You can find additional Help / Tips in the following thread : FAQs and Tips for S5 to S7 Conversion In case you have any specific issues / error that you want further help on, you can post them here. Good Luck Cheers Navnag |
There is no such thing as the last bug in a program |
|
Follow us on