1/7/2016 11:02 AM | |
Posts: 2 Rating: (0) |
Good Moning. I have a situation with CPU319 2 pn/dp. Both Profibus network are at 187 Kbps and I want to create a new profibus Pa network with new CP 342-5 and slaves like flowmetters. If I connect directly in Profibus port with 45.45 kb and Dp/Pa link, transparent, i see the slaw Prowirl 73, adress 5. If I want to add new cp in hardware (cp342-5 ), after PLC, and create new network profi 45.45 kbs I have no communication and the cp is in error like FDL not configured and I hink I cannot create the third Profibus PA network. Can somebody help me with an example for creating the third network. I found an example with im 153-2, to be inserted like slave in existent Profibus network, and split network and the im link, can comunicate at 45.45kbs. Regards, ------------------------------------------------------------------------------------------ |
Last edited by: CatalinStan at: 1/7/2016 11:24:11 AMLast edited by: CS Moderator at: 1/7/2016 11:29:37 AMNew subject after splitting |
|
1/7/2016 11:41 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051) |
hi Catalinstan, your question is a little bit confusing. you are talking about a 319 and a CP 342 and "both PB-Networks" of 187,5kb. In the picture you have a 317 without a CP and only one network. but you are looking online to a flow meter, I guess, that in the one DP-network. I think it is easier to do it like in the example you already found. regards, |
FCK WAR! |
|
1/9/2016 3:25 AM | |
Joined: 10/7/2005 Last visit: 5/3/2024 Posts: 3004 Rating: (1046)
|
Hello CatalinStan
If not, have a look at the FAQ collection below which contains a wealth of useful things to be aware of when using a CP342-5: |
Cheers |
|
This contribution was helpful to1 thankful Users |
Follow us on