2/22/2022 8:32 PM | |
Joined: 4/9/2020 Last visit: 10/7/2024 Posts: 22 Rating: (0) |
Hello, I have following configuration: PS407 10A 6ES7 407-0KA01-0AA0 CPU 416F-2 6ES7416-2FP07-0AB0 CP 443- 1 Adv – IT 6GK7443-1GX30-0XE V3.2.17 CP 443-1 Advanced-IT not going to run mode, but it is showing ‘Stop’ as well as in ‘INTF’ fault. The module buffor shows event: Module database invalid (Internal cause: 8702) I was try download new hardware, general reset of the CPU memory, reset CPU to factory state, new project only with hardware download and the module still not going tu run mode. I only get into run mode in the following way: - power on - connect directly to gigabit interface of CP - go accessible devices - assign IP address - power off - power on - connect directly to profinet interface of CP - go accessible devices - assign IP address - and now the module go to Run mode But if i restart supply the module again not going to run mode, and sometimes ip addresses are still assigned to the interfaces, but sometimes for example gigabit or profinet ip addres is gone. I have attached diagnostic buffor of the module. AttachmentDiagnostics1.txt (259 Downloads) |
2/23/2022 8:30 AM | |
Joined: 4/9/2020 Last visit: 10/7/2024 Posts: 22 Rating: (0) |
Hello, The CPU firmware is V 7.0.2. So i think is the newest. |
2/23/2022 8:44 AM | |
Joined: 4/9/2020 Last visit: 10/7/2024 Posts: 22 Rating: (0) |
Only errors related to profibus communication are present in the CPU buffer. Because two slaves are not connected yet. I have attached diagnostic buffor of CPU. Maybe C-Plug is broken? AttachmentDiagnostics2.txt (302 Downloads) |
Follow us on