6/1/2010 9:49 AM | |
Posts: 76 Rating: (1) |
Simatic Net 206 HF3 Windows Xp SP3 WinCC 6.2 SP3 After every reboot this thing happens. And I need to add this component witth button "Add" |
6/1/2010 10:05 AM | |
Joined: 4/24/2006 Last visit: 5/3/2024 Posts: 8632 Rating: (1148) |
Dear rusgaz, Please have a look at this link: Which SIMATIC NET software component is enabled for which operating system? It could be a compatibility problem Best regards, Wizard |
6/1/2010 10:42 AM | |
Posts: 76 Rating: (1) |
But it works when i add Cp1613 in SCE. Only after rebbot it dissappers. Maybe I've mistaken when i configure it in configuration console? |
6/1/2010 2:16 PM | |
Joined: 12/9/2009 Last visit: 4/18/2024 Posts: 156 Rating: (11) |
Hello, your system is compatible. Have a look at the following link: http://support.automation.siemens.com/WW/view/en/21927773 I suggest you to contact the SIEMENS technical support to solve the problem. Perhaps there is another Hotfix for SIMATIC NET Edition 2006 which solves the problem with CP1613 and Station Configuration Edition: Support Request Best Regards Little Holmes |
This contribution was helpful to1 thankful Users |
6/1/2010 2:26 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181)
|
Hello, Your type of PC is not the same, but could be your type has the same behavior. When you restart, BIOS do not like CP. Box PC 620 / Panel PC 670 - after installing a CP 1613 / CP 5611 Microsoft Win 2000 no longer starts or Windows shuts itself down Or check the settings in CP1613 like PC - S7 Best regards, Hristo Mihalev |
Follow us on