8/15/2014 4:56 PM | |
Joined: 3/20/2013 Last visit: 3/9/2023 Posts: 676 Rating:
|
Normaly it shoudl be no problem to use an older projected version. you will afaik only skip the new features. have a look here: http://support.automation.siemens.com/WW/view/en/81661875 |
Best Regards, |
|
8/15/2014 5:33 PM | |
Joined: 12/14/2010 Last visit: 8/16/2023 Posts: 116 Rating:
|
Hi Fafner, Thanks for clearing my doubt.
|
3/18/2015 5:07 PM | |
Posts: 3 Rating:
|
Hi friend I'd like to get the GSD for the CP443 v7.0. I can't find it on the site. |
3/18/2015 6:00 PM | |
Joined: 9/27/2006 Last visit: 9/22/2023 Posts: 12152 Rating:
|
Hello as3; A gsd file is useful when you need to setup a DP slave as part of a DP master's configuration. The CP 443-5 Extended cannot act as a DP slave, only as a DPV1 master, or a Partner for HMI/SCADA applications, or S5 communications; so no gsd file is available for it. See the following link from Siemens' Industry Mall (electronic catalog): CP 443-5 Extended : DP master only Hope this helps, Daniel Chartier |
Follow us on