1/18/2015 6:40 PM | |
Posts: 1058 Rating: (93) |
Hello diosnel, it could work, as both CPUs are same family. Just be aware that CPU 102 has lower limits in many ways than CPU 103. For example: Markeraddreess from 0.o to 127.7 for CPU 102 Markeraddreess from 0.o to 255.7 for CPU 103 Counter 0 to 31 for CPU 102 Counter 0 to127 for CPU 103 Timer0 to 31 for CPU 102 Timer0 to 127 for CPU 103 if your program does not make full use of CPU103, especially from memory, it could work. See here for technical details of CPUs S5-100U , unfortunatelly in German only. regards |
1/19/2015 4:06 AM | |
Joined: 11/21/2007 Last visit: 9/25/2024 Posts: 2325 Rating: (308)
|
Hello diosnel Well. I would doubt that you would be able to use a CPU 102 in place of CPU 103 in most cases ( Unless of course that the CPU 103 was un-necessarily used where CPU 102 was sufficient ) Although the two belong to the same family as correctly pointed out by eisenpferdreiter, there are major differences besides thouse already pointed out : Memory : CPU 102 : 2048 Statements , CPU 103 : 10240 Statements Blocks( PBs / FBs, DBs) : CPU 102 : 0-63 , CPU 103 : 0-255 No of Operations Supported : CPU 102 : 60 , CPU 103 : 180 Attached pl find Technical specifications ( English ) of CPU 102 and CPU 103 Hope this helps Cheers Navnag AttachmentCPU102_103.pdf (355 Downloads) |
There is no such thing as the last bug in a program |
|
This contribution was helpful to2 thankful Users |
1/20/2015 10:30 PM | |
Posts: 1058 Rating: (93) |
Hello Navnag, I totally agree with you. As you said it would only work, if CPU 103 was un-necessarily used. And during almost 30 years of commissioning I have seen many systems like that. So diosnel will have to check the software, if it is within limits of CPU 102. regards |
Follow us on