Industry Online Support
Technical Forum
10/17/2012 10:23 AM | |
Posts: 559 Rating: (87) |
Dear All, I am facing one problem with S7-200 CPU 226. The program was developed in IEC 1131-3 language. In Network instruction We have division of real values, So actual running program in PLC which was loaded by original programmer is working fine & gives output of real correctly. But the same program we have uploaded & downloaded to other same PLC then it shows output of real Division as '0' value. So please help me how could we get the exact value as it was running to original PLC? Please find the attached program backup for the same. We are facing problem at network-1. The division of VD 1096 & VD88 is coming '0' value at VD 3758. AttachmentIEC 1131-3.zip (157 Downloads) |
10/17/2012 2:26 PM | |
Posts: 559 Rating: (87) |
Dear marwanco62, We are sure that value in VD 88 is not zero. it is something arround 0.8. But our problem is that we are giving value as real & after division we are getting value as DINT. So please clear our this point. why this is happening? |
Follow us on