9/19/2008 8:56 AM | |
Joined: 4/24/2006 Last visit: 1/14/2025 Posts: 8804 Rating: (1173) |
Dear aante, The amount of data will be projected in Master. You can send and receive data using FC1 DP_send and FC2 DP_Recv. See following link: http://support.automation.siemens.com/WW/view/en/21628604 And perhaps this link is useful: http://support.automation.siemens.com/WW/view/en/15007089 Best regards, Wizard |
9/19/2008 9:15 AM | |
Posts: 1064 Rating: (72) |
http://support.automation.siemens.com/WW/view/en/1158693 Check out the manual fo rthe cp 342-5 card it will tell you how to set it up ,the data word size is set up in the FC DP_SEND, FC DP_RECV up to 2000 bytes which is with in your range |
9/19/2008 9:16 AM | |
Joined: 4/24/2006 Last visit: 1/14/2025 Posts: 8804 Rating: (1173) |
Dear aante, Well I guess the master CPU has an integrated Profibus Here is a link about differences between integrated Profibus and CP342-5: http://support.automation.siemens.com/WW/view/en/21628388 http://support.automation.siemens.com/WW/view/en/689920 When you have integrated Profibus, you can use MOVE a range of DW-words to PQW. But when you use CP342-5 you mustuse FC1 and FC2 So there is no possibility, you can do the same as master CPU. (if you wish, you should use CPU with integrated profibus) Best regards, Wizard |
9/19/2008 9:27 AM | |
Posts: 55 Rating: (0) |
yes wizard, the other side is cpu 315-2dp.... if i use fc1 and fc2 on my side, can master side use just move? |
9/19/2008 9:45 AM | |
Joined: 4/24/2006 Last visit: 1/14/2025 Posts: 8804 Rating: (1173) |
Dear aante, It's no problem. The other side can use MOVE instruction Here I found an example: http://support.automation.siemens.com/WW/view/en/6518938 Unfortunately it's the other way around. CP342-5 is master and CPU is slave. But perhaps it's useful Best regards, Wizard |
9/19/2008 9:50 AM | |
Joined: 4/24/2006 Last visit: 1/14/2025 Posts: 8804 Rating: (1173) |
Dear aante, YES, I found another example: http://support.automation.siemens.com/WW/view/en/6519580 CP342-5 is slave and master is CPU. Best regards, Wizard |
9/19/2008 10:05 AM | |
Posts: 55 Rating: (0) |
wizard thank you very much! you make me clear about some things if i have some other questions i will feel free to ask thanx again |
9/19/2008 11:57 AM | |
Joined: 4/24/2006 Last visit: 1/14/2025 Posts: 8804 Rating: (1173) |
You are welcome I'm glad I could help. Best regards, Wizard |
Follow us on