1/28/2011 7:13 PM | |
Joined: 1/28/2011 Last visit: 10/13/2023 Posts: 1 Rating: (0) |
What was the result of this? We have a similar situation with a CPU 317-2 PN/DP connecting with a Micro Motion Mass Flowmeter (see attached screenshot). The manufacter says the GSD file has been certified (see attached gsd). The strange thing is the device expects 10 slots but the HW Config screen in Step7 shows 20 slots. If I change the gsd file such that Max_Module is 5 instead of 10, then the HW Config screen in Step7 shows 10 slots instead of 5 and I get an error when I configure the 6th slot. Splitted from S7-315-2DP Profibus Master => Non Siemens Profibus Slave . |
Last edited by: O_Moderator at: 1/30/2011 10:34 AMnew subject after splitting |
|
Follow us on