5/27/2022 3:41 PM | |
Joined: 2/10/2010 Last visit: 6/20/2024 Posts: 77 Rating: (0) |
Hello mopS04, In an old conversationCP 443-5 Ext fails and cpu goes to stop mode, I see that the CPU went to STOP mode when the CP443-5 fails. This is a case report. But, I would like to be sure whether it is confirmed or not, that the CPU will go to STOP mode in case the Master port available onboard or the CP443-5 fails/gets damaged. Thanks, |
Follow us on