6/29/2019 9:39 PM | |
Joined: 9/27/2006 Last visit: 5/3/2024 Posts: 12257 Rating: (2666) |
Hello destructo; The part number you are showing (6ES7400-4R1 ) is a bundle offer, described in the following discussion; can you confirm that the elements described are the actual part numbers you are using in your project?: If the part numbers are correct, the CPU 6ES7412-5HK06-0AB0 is still active, and can accept the active Modbus TCP drivers from Siemens. For example, you could use: Open ModbusTCP PN redundant : 6AV6676-6MB10-0AX0 H-CPU with integrated PROFINET interface to third-party devices All variants of the Modbus TCP drivers for S7-300 and 400 CPUs are shown here; https://support.industry.siemens.com/cs/ww/en/view/22660304 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 06/29/2019 21:44:14Last edited by: dchartier at: 06/29/2019 22:54:55 |
|
This contribution was helpful to1 thankful Users |
6/30/2019 11:16 AM | |
Posts: 3093 Rating: (322)
|
Which technical data applies for the SIMATIC Modbus/TCP blocks and for which CPUs and CPs is it released? |
This contribution was helpful to2 thankful Users |
Follow us on