Industry Online Support
Technical Forum
3/26/2008 8:34 AM | |
Posts: 196 Rating: (12) |
We have created some functions blocks that we want to use several times in our programs.Now we talk about is possible to implement the alarms from the block, so they can be sent directly to our winCC flex application alarm windows , without we have to create the alarms text in the winCC flex program. E.g. “Pec1Blok” or “Pec1Broken” where “PEC1” is the name on my DB, and “Blok” and Broken” is the alarm from the DB.As I understand it there more than one solution. I can create alarms with sfc107/108 but it seems to have some limitation on the text. Then I have the text library in my block folder according to the manual I can handle different alarms text but I can find any example how to do this. I have look at this faq http://support.automation.siemens.com/WW/view/en/24013249, but I can’t see hov they have use the text library. |
Follow us on