10/25/2018 10:51 AM | |
Joined: 10/11/2006 Last visit: 11/8/2024 Posts: 5935 Rating: (815)
|
Hello, if I understand correctly, you have a cross cutter drive to be replaced and a line feeder with some other drive, but with an encoder feedback, which can be connected to the cross cutter drive? In this case the S120 Cross cutter with DCB Extension could be used. If I'm right with the line feed, you can use the Cross cutter application with CU310-2 and PM240-2 AC/AC drive and interconnect the line feed encoder like a measuring wheel. If you want to operate line feed and cross cutter, a CU320-2 with Booksize Infeed and Motor Modules for both axis could be used. Details can be found in the linked application description. |
With best regards, |
|
This contribution was helpful to1 thankful Users |
Follow us on