5/14/2015 3:50 PM | |
Posts: 93 Rating:
|
Hi all, I have two S7-400 CPU 1) CPU416-2DP (6ES7 416-2XK04-0AB0) 2) CPU412-2DP (6ES7 412-2XG04-0AB0). I checked in CPU data sheet, both cpu maximum range of timer is T0 to T2047 and counter is C0 to C2047. in my program cross reference timer and counter visible only few timer and counter. my doubt is how to increase the C and T range upto maximum in cross reference. where is the setting for change the C and T range. And also input,output,bit memory(visible only few bits) how to see the maximum range of avilability spare in cross reference. here i attached my cross reference snap,pls go through and give some guidence. Advance Thanks & Regards, Suryamuni. Attachmentcross reference timer and counter.pptx (203 Downloads) |
5/14/2015 9:48 PM | |
Posts: 1058 Rating:
|
Hello Suryamuni, cross reference will only show Timers and Counters that are actively used.
regards |
Follow us on