1/26/2011 10:06 AM | |
Posts: 2 Rating: (0) |
hello, i'm using a CU320-2 to control 2 motors in a master-slave composition. Now i make one run in Jog. And the jog positionning setpoint of motor 1, i use as MDI positionning setpoint for the second motor. With DCC software i can make that they always come together in the end. But while running, the slave always stays behind the master untill the master stops and they come together; Both motors have an incremental encoder. (homing is no problem) you can find my program below AttachmentGelijkloopVolvo_AfgewerkteVersie.zip (202 Downloads) |
Last edited by: Pol Meire at: 1/26/2011 10:07 AM |
|
4/15/2011 8:20 AM | |
Joined: 9/18/2006 Last visit: 9/2/2024 Posts: 591 Rating: (64) |
Hi. I have not understood a question not much. If you use MDI that you write down in p2643 Motor_Links? It is my example alternate Master-Slave using DCC. Both drives in mode MDI. Best regards. AttachmentMaster_Slave_DCC.zip (222 Downloads) |
Follow us on