8/15/2019 3:50 PM | |
Joined: 4/28/2015 Last visit: 9/20/2022 Posts: 1278 Rating: (298) |
Hi, performance runtime license is needed if you want to run more than 3 axes on one CU320-2. So up to 3 axes it is not needed, from 4 or more axes it is needed (it has nothing to do with the infeeds). The latest firmware is FW5.2HF4 - here you can download it and copy it to your CF card (so you can also buy a CF card with older FW and replace it by that new files easily): https://support.industry.siemens.com/cs/ww/en/view/109762626 |
Last edited by: RB91 at: 08/15/2019 15:50:43Best regards, |
|
This contribution was helpful to1 thankful Users |
8/15/2019 4:13 PM | |
Joined: 4/2/2016 Last visit: 7/13/2022 Posts: 413 Rating: (6) |
thank you very much!!! Do I understand correctly that if I plan to use one CU320-2 PN to three SLM (SMART LINE MODULE) (parallel connection) it counts as one axis not three? but in what documentation can I read "performance runtime license is needed if you want to run more than 3 axes on one CU320-2." |
2/26/2021 3:42 PM | |
Joined: 10/18/2020 Last visit: 6/25/2024 Posts: 2 Rating: (1) |
Look at the PM21 2013 page 13/12 |
Follow us on