Industry Online Support
Technical Forum
12/21/2013 10:49 AM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating: (709) |
Hi Eng. Mohamed, 1 - Select the folder in Simatic Manager "blocks" can be found in the addresses you want to rewire, then select the menu command Tools ----> Rewire. 2 - On this CPU does not have the MMC but the MC big blue, the one to the left: Which memory cards can you use with an S7-300 CPU? and please hakea look: What is the effect of the STEP 7 function "Copy RAM to ROM"?
3 - when you have the program stored in the MC / MMC card you can make a copy of it, if luck should be damaged "rare case", and CPUs that have the battery change at least once a year. |
This contribution was helpful to1 thankful Users |
Follow us on