9/27/2022 7:39 PM | |
Joined: 3/1/2021 Last visit: 2/6/2024 Posts: 8 Rating: (0) |
Dear, Is there any way to save data in a file that is located on the load memory that also can be read? |
9/28/2022 9:32 AM | |
Joined: 3/11/2019 Last visit: 9/6/2024 Posts: 1569 Rating: (289)
|
Hi, there are instructions "FileWriteC", "FileReadC" and "FileDelete" available. These are not limited to DataLogs. I did some tests in the past and it also worked with files created outside of the cpu - as long as file type, used format ist correct and the file is located in correct folder of SMC. Maybe this can be helpful. Program example for file handlingregards sancruz |
Feedback appreciated, please rate |
|
This contribution was helpful to2 thankful Users |
Follow us on