3/23/2009 8:14 AM | |
Posts: 3 Rating: (0) |
Since install the new version of S7 v5.4+SP4 to me, along with the WinCC Flexible's version 2008, when I attempt erasing a project from the Simatic Manager this it is not able to erase it. Somebody would be able to help oneself to solve this little inconvenience. Thanks for your attention. AttachmentUndeleting s7 Projects.pdf (90 Downloads) |
3/23/2009 8:30 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello Look at Which meaning have the error codes (xxxx:yyyy) in STEP 7? (look for 258:15) Hope his will helps. regards |
3/23/2009 9:53 AM | |
Posts: 3 Rating: (0) |
I have added a *.pdf file to my question, in the one that the how-to message that the S7 relating to the problem offers me that has to erase totally the project evidences itself. I have checked the indications of help for this code of error, and I am responsible with all of them, because the instant this error happens, I from the explorer of Windows can erase completely the project's directory. Any idea but? Thanks for your attention. AttachmentUndeleting s7 Projects.pdf (72 Downloads) |
3/23/2009 11:26 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello From link the last remedy for this problem is reinstall Step7. regards |
Follow us on