6/20/2011 4:41 PM | |
Joined: 9/27/2006 Last visit: 9/21/2024 Posts: 12282 Rating: (2684) |
Hello seb; Here is a quick description of the Siemens diagnostics repeater that could help you understand your requirements: Diagnostics RepeaterThe diagnostics repeater for PROFIBUS DP connects PROFIBUS DP segments with RS 485 technology. It also physically monitors the copper bus lines in online mode. If an error occurs, it sends a diagnostic message to the DP master with detailed information on the type and location of the error. The diagnostics repeater is a standard slave. It can be operated on any DP master that supports the standard RD_REC and WR_REC services. To record the topology, you will need either STEP 7 or COM PROFIBUS. https://www.automation.siemens.com/mcms/distributed-io/en/profibus-components/bus-diagnostics/Pages/Default.aspx?HTTPS=REDIR |
6/20/2011 4:46 PM | |
Posts: 1547 Rating: (129)
|
Hello, the diagnose repeater is like a PROFIBUS Slave. There is a simple data structure for some general information via DP V0 available, but the most information you will get using DPV1 acyclic communication. You have to read different records from this device. Depends on the information you want have you have to read different records. More information about the records and the received datastructure you will find in following manual chapter 7.2 http://support.automation.siemens.com/WW/view/en/7915183 regards Rated X |
Follow us on