Industry Online Support
Technical Forum
2/11/2011 8:53 PM | |
Posts: 26 Rating: (1) |
Hi adilmahsan It can be done, but unfortunately it required some hard work. But I will tried to share the knowledge I have regarding to fetch diagnostic data. Me and my colleagues have only testes that we was able to offer a detailed diagnostic system for a customer, but we haven’t received any order yet, so there for I have no full scale experience. Here is the description how to use the SNMP diagnostic in with PCS7. http://support.automation.siemens.com/WW/view/en/18804292 Thisgive you an idea of the concept http://support.automation.siemens.com/WW/view/en/27731583 In the HW configuration you have to create an MIB file for switch, the your able to get a detailed for each port one every switch. All the profile should be save under …step7\s7data\snmp\profile and not the user_profil,e because when we tried it the hardware compiler failes. This file contains the link between the status “word” from the switch and all alarm texts is stored here. step7\s7data\snmp\snmp_in\s7snmpalarm.xml Contains the link between from the snmp profile to the alarm texts step7\s7data\snmp\snmp_in\s7snmp.xml I have attach the profile we have made for scalance X3** and scalance R switche. Tried to reverse engineer my files. Please note that step7 only will work on this installation because of the modification to the xml files. Personal I could use a better guide (hint for Siemens) how to configure a sclance x switch with the snmp OPC editor we only got this to to work because of hard work and luck. And the online help for the snmp interface s…. I anyone has an easier method ore can fill out some gaps in my post pleas do it. Pleaselet me know you get i to work. // Bedst regards // Søren C. Attachments7snmp.zip (59 Downloads) |
This contribution was helpful to2 thankful Users |
2/16/2011 3:15 PM | |
Posts: 26 Rating: (1) |
Hi No sorry, but I think maybe you look in the xml files. // Søren C. |
Follow us on