Industry Online Support
Technical Forum
1/17/2011 3:35 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365) |
Dear member Two well known options are: 1-PLC-ANALYZER pro 5 2- ibaPDA Wincc from SIEMENS also provides data aquisition of at least 500ms in normal cases(e.g in S7300). The following codes transfer the status word to a memory for checking [code]L STW T MW0[/code] BIT #0---> /FC BIT #1---> RLO BIT #2---> STA BIT #3---> OR BIT #4---> OS BIT #5---> OV BIT #6---> CC0 BIT #7---> CC1 BIT #8---> BR BR |
Last edited by: hdhosseini at: 1/17/2011 3:42 PM |
|
Follow us on