3/2/2020 5:23 AM | |
Posts: 114 Rating: (2) |
Dear All, Can I use I-Device Instead Of Get-put. Is There Any Drawback Of I-Device Compared To GET-PUT |
3/3/2020 1:26 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050)
|
hi vicky bhau, communication whit PUT/GET needs a S7-connection between two S7-Controller, over S7-protocol. have a look to these application sample: How do you configure and program an S7 connection and the "PUT" and "GET" instructions for data transfer between an S7-1500 CPU and an S7-1200 CPU?
I-Device is Profinet-communication. therefore one of the controller ist device to the other controller. have a look to these application sample: Configuration and Application of the PROFINET I-Device FunctionThere are much more application samples an FAQ to these two communcation methods. I also recommend this manual about CPU/CPU communiation with Simatic Contollers. hope this helps, regards |
FCK WAR! |
|
Follow us on