8/22/2019 4:13 PM | |
Joined: 5/6/2019 Last visit: 9/12/2023 Posts: 78 Rating: (0) |
Hello I am trying to connect SINAMICS S120 CU310-2 PN V4.8 with safety program to S7 1500 PLC. After going online I am getting the error from PLC as follows, MC alarm 421: Drive under logical address 23 faulty. Alarm message from drive. MC component: PositioningAxis_1, TO_DB= 2 The error from drive is as follows, Module exists. Error Additional information for the module: Differences were found between the loaded configuration and the offline project. Online article number: 6SL3 040-1LA01-0AA0 Offline article number: 6SL3 040-1LA01-0AAx I referred to the topic here,https://support.industry.siemens.com/tf/ww/en/posts/differences-were-found-between-the-loaded-configuration-and-the-offline-project/177905/?page=0&pageSize=10 I noticed that my drive is 5.1 version and hence installed the gsdml file for the same from https://support.industry.siemens.com/cs/de/en/view/49217480 After compilation adn loading also I am getting the same error. On further check, it can be noticed that the error is coming from the Telegram 30 of the drive. I am attaching the image of error here. PS: I am using Starter for the configuration of the Drive. My TIA version is 15. Any help would be appreciated to solve this problem. Regards, Bindu Attachmentplc_drive.pdf (66 Downloads) |
Last edited by: Jen_Moderator at: 08/23/2019 10:24:47Optimized link. |
|
8/26/2019 11:59 AM | |
Joined: 5/6/2019 Last visit: 9/12/2023 Posts: 78 Rating: (0) |
Thank you for the points to check.. My online version number are now same as GSDML file. I am sttaching the screenshot. May I know what is the order of the telegramm. I am attaching a screenshot of that too. AttachmentComparison.pdf (86 Downloads) |
Follow us on