4/19/2011 11:02 AM | |
Joined: 10/7/2005 Last visit: 5/3/2024 Posts: 3004 Rating: (1046)
|
Hello faizee you almost answered your own question when you stated that "...Iguess it can be happen with S7300 series when using with PCS7 as PCS7 is mainly designed for S7400 series". As far as I'm concerned PCS7 is not "mainly designed for S7 400" but ONLY designed for S7 400 and NOT relased (nor supported) with S7 300 PLC's. You'll also find that a fair few of the PCS7 related S7 Blocks use SFC's and SFB's that simply do NOT exist in the OS of a S7 300 CPUand as such have no change to work. I'm afraid to say that the only advise I can give you is to get rid of your S7 300 and use a PCS7 released S7 400 CPU instead. |
Cheers |
|
This contribution was helpful to1 thankful Users |
4/19/2011 11:45 AM | |
Posts: 12 Rating: (0) |
thanks fritz for your explanation |
Follow us on