10/12/2020 7:08 AM | |
Joined: 11/11/2018 Last visit: 2/4/2023 Posts: 5 Rating: (0) |
I used DIGSI V4.94, to change Modbus slave address from GlobalSection.SlaveAddress from "9" to "1" but it's change by DIGSI see picture 1 ok(already changed also I verified by plug and ply is ok come device ID "1", but I checked from "ModScan 32" not connect if I put Device Id "1" and connected if change Device Id to old one "9" I trying by remove Maping and return and not come please urgently reply ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/12/2020 13:06:53New subject after splitting |
|
Follow us on