Industry Online Support
Technical Forum
12/1/2012 7:43 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating:
|
Hello, You have found the right replacement panel, see: Discontinuation of SIMATIC HMI Panels TP 070, TP 170A/B/INOX and OP 170B effective 04/01/2008 But if we look at 6AV6642-0BC01-1AX0TP177B DP MONO you see that one is already cancelled too The succesor is available until end off 2014. 6AV6642-0BC01-1AX1 TP177B 6" DP BLUE MODE The panel can be downloaded with at least Winccflexible 2005, if you have the projectfile of yourTP it can be converted to the new panel. If you have only an uploaded backup, you can only download it to same panel type. Regards, Marcjan |
Problem solved? |
|
Follow us on