7/6/2022 7:13 AM | |
Joined: 3/14/2008 Last visit: 9/13/2024 Posts: 2095 Rating: (936)
|
Hi, If you make sure the signal status is set to 16#80, then it's a "good" status. If your signal is not ok, you can use a StruScIn (FC379) and StruScOu (FC380) block. It's a structure decomposer and composer. With FC379 you decompose a structured signal into a separate BOOL and BYTE. With the FC380 you compose a BOOL and BYTE to a structured signal. Fed the 16#80 on the BYTE signal and then it should be good. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to2 thankful Users |
Follow us on