1/28/2019 9:26 AM | |
Joined: 6/9/2017 Last visit: 7/11/2024 Posts: 3 Rating: (0) |
Hello! Siemens says: "The programming languages of SIMATIC STEP 7 (TIA Portal) meet the requirements of IEC 61131-3" (https://support.industry.siemens.com/cs/ww/en/view/50204938). Unfortunately not in 100%. In this file (http://d1.amobbs.com/bbs_upload782111/files_31/ourdev_569653.pdf) page 33 you can find that IEC 61131-3 allows creating non-structured user data types e.g.: TYPE ANALOG_DATA : INT (-4095..4095) ; END_TYPE I have prepared External Source File containing such line but TIA cannot generate udt. If I remove range "(-4095..4095)". It generates ANALOG_DATA type but its empty. In the other file I found that TIA allows only STRUCT in UDTs. Conclusion is: SIMATIC STEP 7 (TIA Portal) meet the requirements of IEC 61131-3 but not in 100%. Am I right? If not please correct me? Best regards! Attachmentourdev_569653.pdf (159 Downloads) |
Last edited by: Jen_Moderator at: 1/28/2019 2:34:48 PMOptimized link and added PDF as an attachment. |
|
Follow us on