6/23/2014 9:27 AM | |
Posts: 4 Rating: (1) |
When I select to download an entire WinCC project to the primary server of a redundant OS pair, it gives the following message: Project \\servername\projectname.mcp is activated on the target system \\servername. Do you want to deactivate and close this project? I then choose YES and the dialog box in the right hand corner shows preparation for the download. However, at the point where the project needs to be deactivated, the dialog box just disappears and nothing further happens. I do not have the same problem with the standby server of the redundant pair. It deactivates the project, closes it, downloads, and then reloads and restarts the project without a problem. |
Last edited by: Bucs at: 6/23/2014 9:29 AM |
|
Follow us on