4/2/2024 9:07 AM | |
Joined: 12/15/2022 Last visit: 4/8/2024 Posts: 4 Rating: (0) |
Hello everyone, I'm encountering an issue with the DP/PA Link (6ES7 153-2BA70-0XB0) and could use some assistance. My setup includes four types of devices: Control Valves, Mass Flowmeter, Temperature and Pressure Transmitters. There's no error when configuring Temperature and Pressure Transmitters and up to only one of either Control Valve or Mass Flowmeter. Attempting to add more than one Control Valve or Mass Flowmeter results in the entire DP/PA Link encountering an error. Upon checking the diagnostic buffer, the error message reads "not reachable" AttachmentScreenshot.zip (6 Downloads) |
Last edited by: Ziv Mathieu at: 04/02/2024 09:13:10 |
|
Follow us on