1/11/2022 1:30 AM | |
Joined: 7/28/2021 Last visit: 9/23/2022 Posts: 7 Rating: (1) |
For the example that I made in the flat style button thread., I used button.default.svghmi as inspiration for handling the hmi events internal to the svghmi file. It can be found in the following folder: C:\Program Files\SIEMENS\Automation\Portal V17\Bin\_resources\web\templates\extended\V1600 I'm sure that there are other events besides onMouseDown and onMouseUp, but I haven't looked for them in the included Siemens svghmi files. |
This contribution was helpful to1 thankful Users |
1/11/2022 5:42 AM | |
Joined: 10/19/2021 Last visit: 2/28/2022 Posts: 46 Rating: (2) |
Ah thanks alot! I've only searched inside the svgcontrols folder, where the files don't have an event at all. |
Follow us on