7/26/2019 8:37 PM | |
Posts: 7 Rating:
|
I have this exercise in which there are 5 different scenarios. !) By pressing the first time the push button all 4 outputs are on. 2) Pressing the second time makes the 2 and 3 outputs off. 3) Pressing the third time makes the 1 and 4 outputs off. 4) The forth time cause the output 4 on and with 3s intervals the rest of the outputs start to be on ( after 3s output 3, after 6s output 2 and after 9s output number 1). 5) At last pressing the push button leads to output 1 off and with 2s intervals the rest of the outputs start to be off ( after 2s output 2, after 4s output 3 and after 6s output number 4). I managed to developed these scenarios but now I want to avoid any interference within these 5 scenarios ( For example when it is in the 4th stage does not allow to go further unless the 4th stage is accomplished.) I would be more than grateful if anyone has any suggestion. AttachmentFiles.zip (188 Downloads) |
7/27/2019 5:32 AM | |
Joined: 12/18/2014 Last visit: 8/6/2024 Posts: 33498 Rating:
|
In attachment a possible solution with a step sequence. The OR blocks at the terminals of the latching relays are not mandatory. AttachmentScenario_FS4.zip (215 Downloads) |
7/27/2019 7:01 AM | |
Posts: 7 Rating:
|
Thank you very much, this is helpful. |
This contribution was helpful to
1 thankful Users |
7/27/2019 7:03 AM | |
Joined: 12/18/2014 Last visit: 8/6/2024 Posts: 33498 Rating:
|
Is your problem now solved? |
7/27/2019 7:41 AM | |
Posts: 7 Rating:
|
Yes it is solved, thank you. |
This contribution was helpful to
1 thankful Users |
7/27/2019 7:43 AM | |
Joined: 12/18/2014 Last visit: 8/6/2024 Posts: 33498 Rating:
|
If a had time today, I make a solution with a shift Register. |
7/27/2019 7:50 AM | |
Posts: 7 Rating:
|
I appreciate your time. |
This contribution was helpful to
1 thankful Users |
7/27/2019 1:15 PM | |
Joined: 12/18/2014 Last visit: 8/6/2024 Posts: 33498 Rating:
|
Attached the version with a shift register.
AttachmentScenario_FS4_V2.zip (217 Downloads) |
Follow us on