1/17/2018 6:11 AM | |
Joined: 4/23/2010 Last visit: 5/7/2023 Posts: 8034 Rating:
|
Hello katoshnik, Encoder ERN 1381 is 1 Vpp interface without Z1 track encoder where as ERN 1387 is 1Vpp with Z1 track encoder. ERN 1381 & ERN 1387 connections are different. Please refer attached sheet for detail information. 6SN1123-1AA00-0CA2 is 50 A single axis power module. Please provide detail MFB number of control module or attach snap shot of LED BR along with card number MLFB to let you know its significance. HTH. |
1/17/2018 7:16 AM | |
Posts: 5 Rating:
|
Thank you, but i have ERN 1381 with 14 pin |
1/17/2018 7:56 AM | |
Joined: 4/23/2010 Last visit: 5/7/2023 Posts: 8034 Rating:
|
Yes, Please refer your attached which mentions pins 5,6 & 4 are not connected for ERN 1381, it is not standard, it is modified i.e. tailored made. Please attach control module snap so as to understand BR LED. |
1/17/2018 11:30 AM | |
Posts: 5 Rating:
|
It's attach from here |
1/25/2019 3:53 AM | |
Joined: 2/22/2016 Last visit: 8/2/2022 Posts: 14 Rating:
|
Ok fine, I got the details regarding 1381 & 1387. But can you read question again & check your PDF attachment you will find some difference, I am also have question like katoshnik, I have encoder ERN 1381 but it has 14 pin connector & in your drawing it's 12 pin connector please describe it properly. |
Follow us on