Industry Online Support
Technical Forum
9/13/2012 1:36 PM | |
Joined: 5/18/2006 Last visit: 10/21/2020 Posts: 170 Rating: (64) |
Please refer to FAQ 43906783, 'How do you select the unit at the block connection of a channel driver block of the PCS 7 APL?'. This FAQ provides instructions and a sample project/library to use enumerations for some of the APL defined engineering units. PCS 7 APL V8.0 Channel driver blocks have been modified to provide the S7_enum attribrute to the units input parameters (so this step of the FAQ is not required for the V8). One must enter in the name of the enumeration containing the engineering units listing. Note: this FAQ is planned to be updated to provide a complete enumeration listing of all APL defined engineering units. Attached is the English version of the complete APL defined engineering units that you can use in the meantime. Just retrieve the project/library and copy the enumeration to your project(s) as required. cabreytj AttachmentC:\PNOUnitsLib2012-08-16.zip (772 Downloads) |
This contribution was helpful to2 thankful Users |
9/13/2012 2:45 PM | |
Joined: 8/23/2012 Last visit: 8/20/2024 Posts: 118 Rating: (4) |
MonAnS - in APL/monitor. Ty for help, i will read this manual . |
This contribution was helpful to1 thankful Users |
Follow us on