1/14/2021 2:20 PM | |
Joined: 2/29/2016 Last visit: 10/17/2023 Posts: 1 Rating: (0) |
Hi, Have you found the solution? Because I am having the same issue with a servomotor 1FK7022-5AK21-1VA3. I am trying to do the commissioning with a S120 drive through Starter... It would be nice if anyone can help. ERROR 7990: drive incorrect motor data identification (103) 103: Maximum frequency exceeded during the rotating inductance measurement. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/15/2021 08:34:12New subject after splitting |
|
1/15/2021 4:29 PM | |
Joined: 7/7/2010 Last visit: 5/14/2024 Posts: 14724 Rating: (2364) |
That Siemens motor, is it a Drive-cliq™ motor? I don't think so. However, if it is a drive-cliq motor and it is not able to perform a motor ID, perhaps you should not do one and see if it performs properly without tuning. If it is not a Drive-Cliq motor, what parameters have been entered during the Starter motor setup wizard? Did you use the nameplate, or the datasheet for that part #? Is it possible this motor has the wrong nameplate? The datasheet provides some specifics which can be measured. What version of Starter are you using, and what firmware in your CU310-2/320-2? Starter commissioning wizard, was your motor available from the list of motors, or did you have to manually enter motor configuration parameters, or both?
|
science guy |
|
3/22/2022 6:08 AM | |
Joined: 9/18/2015 Last visit: 1/18/2024 Posts: 44 Rating: (1) |
I get the same fault. They are siemens drivecliq motor. Can anyone help? 6SL3120-2TE15-0AD0 with Siemens Synchronous motor 1FK7062-2AF71-1QG0 |
3/22/2022 8:01 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello, 6SL3120-2TE15-0AD0 is double motor module 5A/5A capacity. 1FK7062-2AF7.-.... is 1.9 KW motor 8.5 Nm. Please check if the motor is connected to correct port i.e. X1 or X2 of double motor module. |
This contribution was helpful to1 thankful Users |
11/20/2023 12:10 PM | |
Joined: 6/19/2017 Last visit: 5/14/2024 Posts: 8048 Rating: (164) |
Hello Nicolas_Pastuch, welcome to the community! Many thanks for sharing your solution. For the next time, please try to post in English. This is an international community, and we try to focus on one language. This is the translation of your post:
Regards, |
My Forum is the place to personalize your profile, |
|
Follow us on