4/19/2012 10:59 PM | |
Joined: 9/19/2009 Last visit: 4/27/2024 Posts: 458 Rating: (81) |
Everytime I try to transfer my project to the CPU the following error is displayed Unable to copy the block FB2, please see the screenshots attachment I have been following the sample project, so I don´t understand where is the fault, but is obvious I´m doing something wrong Any help is very gratefull Thanks AttachmentPictures.zip (70 Downloads) |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
4/19/2012 11:41 PM | |
Posts: 1064 Rating: (72) |
this is just ag if this is correct ?thought but in your datablock you are showing an array just wonderin |
4/20/2012 11:01 AM | |
Joined: 9/19/2009 Last visit: 4/27/2024 Posts: 458 Rating: (81) |
Hi Mr. Sorry but I don´t Understand what you are trying to tell me with ag. Yes, my datablock is an array, I have been copy from the sample project. I have tried copy all the blocks from sample project and load to my CPU, and always the same error, not is possible to load FB2 Is possible that my old CPU 6ES7 315-2AF03-0AB0 V1.2 don´t souport FB2 P_RCV? Righ now, I´m going to search information about that. I think this is the trouble I found this FAQ http://support.automation.siemens.com/WW/view/en/24533623 Thanks |
Last edited by: JM76 at: 4/20/2012 11:18 AMLast edited by: JM76 at: 4/20/2012 11:17 AMIf my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
4/20/2012 11:53 AM | |
Joined: 9/19/2009 Last visit: 4/27/2024 Posts: 458 Rating: (81) |
Problem solved with the old FB1 P_RCV_OLD1 |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
This contribution was helpful to3 thankful Users |
Follow us on