3/19/2015 1:09 PM | |
Joined: 6/10/2009 Last visit: 10/13/2024 Posts: 45 Rating: (1) |
Dear all, We are using PCS7 V8.1. We have put a project in runtime and it is online with PLCSIM. Ever thing is running fine. This issue is we have to change a setting in Connection parameters. We deactivated the runtime and selected the check mark for Send/receive raw data block. As we click ok we are getting an error as 'Failed to edit the object. Note - The connection is read only' This happen if we change any of the parameters in the connection parameter window. Please see the screenshots attached. Please suggest how can we change the parameters. Thanks and regards, Shailendra. AttachmentError.zip (147 Downloads) |
3/23/2015 2:51 PM | |
Posts: 140 Rating: (7) |
Hello Shailendra, Can i know what is scenario to change the parameter in WinCC? you can change it in netpro and you can use normally. |
10/8/2015 3:54 AM | |
Joined: 4/27/2015 Last visit: 10/16/2024 Posts: 1 Rating: (0) |
Hi all, a
I also encounter the same problem.
Any workaround on this? |
3/5/2018 9:21 AM | |
Joined: 3/14/2008 Last visit: 10/15/2024 Posts: 2111 Rating: (942)
|
Hi all, The option tungpt3149 provided is not available at PCS7 V8.1. I also searched for this option. However with PCS7 V9.0 and possibly PCS7 V8.2 (have to check) it is possible to set the raw data connection during the OS compile as tungpt3149 described... |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on