2/10/2011 2:37 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
I just downloaded the same GSD_GSE_10_2010 zip file. Unziped and successfully installed all GSDs. My version of Step7 is 5.5. I don't think this is important here. At least you could update yours to SP5. Best regards, Hristo Mihalev AttachmentGSD_GSE_10_2010.zip (363 Downloads) |
This contribution was helpful to2 thankful Users |
2/10/2011 3:05 PM | |
Joined: 4/24/2006 Last visit: 5/27/2024 Posts: 8657 Rating: (1154)
|
Dear Wasp, Please in Hardware configuration, close the open project. Then you can install GSD file. how do you integrate a GSD file into the STEP 7 HW Config for PROFIBUS or PROFINET? See point 2!!!! Best regards, Wizard |
2/11/2011 7:54 AM | |
Joined: 10/7/2005 Last visit: 5/27/2024 Posts: 3007 Rating: (1049)
|
Hello Wasp Not too sure what's wrong, the LENZ2133.GSD imports fine when I try it (with Step 7 V5.5) Interestingly enough though, PI's GSD Editor is"complaining" about the LENZ2133.GSD file (see attached pic) and perhaps your Step 7 version does apply different check and rejects it because of this(a simple test wouldbe to change the"GSD_Revision" from1 to 2, note that you'll need to re-import the GSD file into Step 7 afterwards). Alternatively, use the LEN_2133.GSD file, this one has the added advantage that it supports DPV1 (and also works with my Step 7 V5.5). I hope this helps |
Cheers |
|
This contribution was helpful to1 thankful Users |
Follow us on