11/17/2022 9:59 AM | |
Joined: 7/25/2017 Last visit: 5/5/2024 Posts: 297 Rating: (44) |
Hello, if it is possible to post your project here, I can try to replicate the problem and find out what the issue is |
11/17/2022 11:04 AM | |
Joined: 11/17/2022 Last visit: 9/3/2023 Posts: 8 Rating: (0) |
Hello Please find the attached file which i started to create SCL and i received the error message. LAD program is available. Please check the possible error & If possible kindly send me back the same program file by adding sample SCL coding in FB. Thanks AttachmentSample Project.zip (162 Downloads) |
11/17/2022 11:47 AM | |
Joined: 1/21/2013 Last visit: 5/6/2024 Posts: 2745 Rating: (444)
|
Hi abdulwajidd, I have not had any problems creating an SCL block. But you should install Update 6 for TIA Portal V16. Kind regards AttachmentSCL-Sample.zip (207 Downloads) |
11/17/2022 5:54 PM | |
Joined: 11/17/2022 Last visit: 9/3/2023 Posts: 8 Rating: (0) |
Hello I tried to install update 6 in TIA V16, but now i can't able to open the software and i received the application error message as in the attachment with application & system event file. Thanks AttachmentApplication event.zip (188 Downloads) |
Follow us on