1/30/2018 9:50 AM | |
Joined: 4/24/2006 Last visit: 8/7/2024 Posts: 8711 Rating:
|
Hello #dP, Sorry, but can you post mentioned screen Best regards, Wizard |
1/30/2018 10:00 AM | |
Joined: 4/24/2006 Last visit: 8/7/2024 Posts: 8711 Rating:
|
Hello #dP, Have you seen this thread: an-error-occured-while-upgrading-the-project-library-0080-000030 Best regards, Wizard |
1/30/2018 10:36 AM | |
Posts: 2826 Rating:
|
Thank you Wizard for the link
For my work flow I put some code (above is in LAD) in the project library. These are previous versions or code pieces that needs to be trimmed down to what the project needs. The items seem above does not contain any read/write protection. Deleting the items in "Master copies", saving the TIA V13.0.2 project and converting now occurs as planned. I am glad this issue got captured. BR |
This contribution was helpful to
1 thankful Users |
1/30/2018 10:44 AM | |
Posts: 2826 Rating:
|
Wizard - could I borrow your attention to another thread please: There is a video showing the problem. I have reported this at the feedback of the FAQ and there is yet no response. |
Last edited by: #dP at: 1/30/2018 10:46:32 AM |
|
1/30/2018 4:29 PM | |
Joined: 7/7/2010 Last visit: 8/7/2024 Posts: 15068 Rating:
|
I too recently went through an upgrade from V13 SP2 (SP1 in disguise) to V14 SP1. Read up and installed V14 in a VM on Win7-64. Copied project to VM. Opened in V14. Failed. Tried on 3 other computers with V14. All failed. Sent to Support Request who then split the project into pieces. Just PLC. Just HMI. Just library. Compile each in V13 SPx until no errors occur (noting any changes required, like removing know-how protected blocks). Now convert each individual project piece. That went great for the plc after splitting the hmi / library off. The hmi had some issues that did not translate well between versions, so had to compile away all warnings, again noting changes. After compiling success in V13 SPx, V14 conversion went fine. After all 3 pieces compiled in V14, upgraded to V14 SP1, then recombined the 3 pieces into a single project, adding back all the forcibly removed items, reconnecting up the tags in the HMI, and everything was happy again.
|
science guy |
|
Follow us on