12/7/2021 6:45 PM | |
Posts: 257 Rating: (75)
|
Hello SIOS Forum Community, 2 HART analogue input modules can be connected to the ET 200M: - SM331, 8AE, 0/4-20MA HART; 6ES7331-7TF01-0AB0 - SM331, 2AE, 0/4-20MA HART; 6ES7331-7TB10-0AB0 These HART analogue input modules cannot be connected by means of a SIMATIC Top connect connection technology, as the pin assignment of the SIMATIC pin assignment of the SIMATIC Top connect connection system is not compatible with the pin assignments of the modules listed. As a possible solution, various front connectors are available, which can be selected using the TIA Selection Tool, for example. Note The procedure described in this article refers to the time of writing this article (status: December 2021). Yours sincerely SIMATIC International Technical Support Hub |
Last edited by: SIMATIC International Technical Support Hub at: 01/17/2022 19:22:00 |
|
Follow us on